FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > CPU Module > Regarding differences between 8 bit and 16 bit modes for non-protocol communication
FAQ
Regarding differences between 8 bit and 16 bit modes for non-protocol communication
Please tell me how to use 8 bit mode and 16 bit mode when using non-protocol communication.
Answer
In 8-bit mode, the upper 8 bits of transmitted and received data are ignored and only the lower 8 bits are valid data.
In 16 bit mode, send/receive data is divided into lower and upper 8 bits.
In 16 bit mode, send/receive data is divided into lower and upper 8 bits.
If the external device you want to communicate with sends and receives data in 8-bit units, you can also set the PLC to 8-bit mode so that there is no need to divide the received data after sending and receiving.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Network/Communication
- Series
- MELSEC iQ-F Series