FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding Cloud Connectivity
FAQ
Regarding Cloud Connectivity
Is it possible to connect to the cloud with the iQ-F series?
Answer
It is possible to connect to the cloud: MQTT broker (server) using the MQTT communication function of FX5-ENET.
The MQTT communication function is supported in the following versions.
・Hardware serial number: 234 **** or later
・Firmware version 1.200 or later
The MQTT communication function is supported in the following versions.
・Hardware serial number: 234 **** or later
・Firmware version 1.200 or later
- Product Name
- FX5-ENET
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series