- No : 23612
- Release Date : 2018/09/14 15:09
- 
          
              Print
          
        
 
BUSY signal
    
      Does the BUSY signal turn ON when position control of movement amount "0" is executed?
    
  
    - Category : 
- 
      
    
 
    Answer
  
    The BUSY signal turns ON even when position control of movement amount "0" is executed.
However, since the ON time is short, the ON status may not be detected in the sequence program.
  
    
      
        - Product Name
- Simple Motion module/
 Positioning module
        - Series
- MELSEC iQ-R
 MELSEC iQ-F
 MELSEC-Q
 MELSEC-L