- No : 23620
 
      - Release Date : 2018/09/14 15:09
 
        - 
          
              Print
          
        
 
  
 
Servo motor rotation direction
    
      I've changed the motor direction setting, but the motor is not operating in the set direction.
How can I reflect the change? 
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    To reflect the change, set "[PA14] Rotation direction selection/travel
direction selection" and cycle the servo amplifier or execute a home position return after resetting the controller.
  
    
      
        - Product Name
 
          - Simple Motion module/
Positioning module 
      
      
        - Series
 
          - MELSEC iQ-R
MELSEC iQ-F
MELSEC-Q
MELSEC-L