Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 20764
  • Release Date : 2018/08/21 16:10
  • Update : 2018/09/04 16:20
  • Print

About the tropical treatment

Answer

Products get exposed to environments of elevated humidity when they pass through tropical areas. We do varnish processing to prevent insulation degradation. Paste the exclusive nameplate on the processed product.
Product Name
Geared Motors
Series
Geared Motors Parallel shaft type, Geared Motors Right angle shaft type, S-PM Geared Motors Parallel shaft type, S-PM Geared Motors Right angle shaft type
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?