Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 20778
  • Release Date : 2018/08/21 16:10
  • Print

Differences between flange and face mounting

Please explain the difference between flange and face mounting patterns.
Category : 

Answer

SHY right angle shaft type has lineup of flange and face mounting. For face mount type, screw hole processing is done on the flange surface of the gear case, and flange type is counterbored hole processing is done.
Please select according to the installation method of the equipment.
Product Name
Geared Motors
Series
Geared Motors Right angle shaft type, S-PM Geared Motors Right angle shaft type
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?