FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Output signal
FAQ
Output signal
Are there any restrictions on the wiring length of the output terminal RUN and relay terminal ABC?
- Category :
Answer
The length within 30 m is recommended. When the wiring length is long, signals may not be received accurately due to the increased inductance.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800, FR-D700, FR-E700, FR-E700EX