FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > Inverters-FREQROL > FR-PU07
FAQ
FR-PU07
Can I connect the FR-PU07 to FR-A800/F800 directly?
- Category :
Answer
No. They can be connected with the connection cable (FR-CB20[]). [] indicates cable length (1 m, 3 m, 5 m).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800, option