FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > DC reactor
FAQ
DC reactor
Can I use the DC reactor 75K or higher enclosed with the A700/F700P?
- Category :
Answer
It can be used since the specifications are the same. Note that the warranty period and expected lifespan for the A700/F700P are inherited.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800