FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Reverse rotation prevention selection
FAQ
Reverse rotation prevention selection
When the reverse rotation is disabled by Pr.78 = 1 and rotation direction at restart is enabled by Pr.299 = 1, does the inverter perform reverse operation?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
Yes, it does. When the inverter is coasting in the reverse direction, it starts in the reverse direction and switches to the forward rotation after a deceleration stop.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700, FR-D700, FR-E700, FR-F700, FR-F700P, FR-F700PJ