FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Amount of heat generated
FAQ
Amount of heat generated
How much heat does the FR-A700 series generate?
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
Refer to the FR-A700/F700/E700/D700 series TECHNICAL MANUAL (section 3.7.2) and the Technical News. The FR-A700/F700/E700/D700 series TECHNICAL MANUAL can be downloaded from the Mitsubishi Electric FA Global Website. - FR-A700/F700/E700/D700 series TECHNICAL MANUAL Select FA HOME > Inverters-FREQROL > Technical manual (It is displayed by clicking "Select large category".) FR-A700/F700/E700/D700 series TECHNICAL MANUAL: SH-060014 - Technical News FA HOME > Inverters-FREQROL > Technical library > Technical news MF-Z-078: FREQROL-A700 series amount of heat generated (Amount of heat generated for other models are also described.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700