FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Parameter setting
FAQ
Parameter setting
Can I input the single-phase 200 V only when setting the parameter of the inverter?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
Yes. The single-phase 200 V can be input.
If the single-phase input is performed when Pr.872 (Input phase loss protection) is set to "1", the input phase loss (E.ILF) error may occur, but the parameters can be set.
If the single-phase input is performed when Pr.872 (Input phase loss protection) is set to "1", the input phase loss (E.ILF) error may occur, but the parameters can be set.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700