FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Motor coasting
FAQ
Motor coasting
How can I set the motor to coasting state?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
To set the motor to coasting state, the following methods are available: 1. Set Pr.250 (Stop selection) to "0" and turn OFF the start command.
2. Short the terminals MRS and SD.
2. Short the terminals MRS and SD.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700