FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Printing (character size) of FR-Configurator
FAQ
Printing (character size) of FR-Configurator
The parameter list is printed in small characters in FR-Configurator (FR-SW3-SETUP-WJ) Ver.2.00.
Can I print it in big characters as with FR-SW1 and FR-SW2?
Can I print it in big characters as with FR-SW1 and FR-SW2?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
The size of the fonts are bigger to make it easy to read in Ver.2.01 of FR-Configurator (FR-SW3-SETUP-WJ).
Download the latest version from the Mitsubishi Electric FA Global Website for update.
Download the latest version from the Mitsubishi Electric FA Global Website for update.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700