FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Frequency setting
FAQ
Frequency setting
I want to change the output frequency. Is it changed by changing the setting of Pr.1 (Maximum frequency)?
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
The output frequency is not changed by the maximum frequency setting.
It can be changed by the following methods.
- Set the frequency on the operation panel.
- Set the frequency (terminal 10-2-5 connection) with the potentiometer (frequency setting potentiometer).
- Set the frequency (terminal 4-5 connection) with the current output device (4 DC to 20 mA).
- Change the frequency to the one set in the parameter in advance by turning ON/OFF the switch connected to the terminal. (Multi-speed setting: terminal RH, RM, RL etc.)
It can be changed by the following methods.
- Set the frequency on the operation panel.
- Set the frequency (terminal 10-2-5 connection) with the potentiometer (frequency setting potentiometer).
- Set the frequency (terminal 4-5 connection) with the current output device (4 DC to 20 mA).
- Change the frequency to the one set in the parameter in advance by turning ON/OFF the switch connected to the terminal. (Multi-speed setting: terminal RH, RM, RL etc.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700