FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Electronic thermal O/L relay setting
FAQ
Electronic thermal O/L relay setting
Multiple (five) motors are connected to a single inverter.
Since the rated current of a single motor is 1 A, can I set Pr.9 (Electronic thermal O/L relay) to 5 A?
Since the rated current of a single motor is 1 A, can I set Pr.9 (Electronic thermal O/L relay) to 5 A?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
When using multiple motors, connect an external thermal for each of them.
Set Pr.9 to "0" to disable the function. (When multiple motors are present, it is not clear which motor has large current flowing.) The inverter can only see the total current.)
Set Pr.9 to "0" to disable the function. (When multiple motors are present, it is not clear which motor has large current flowing.) The inverter can only see the total current.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700