FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Frequency setting
FAQ
Frequency setting
As Pr.7 (Acceleration time) and Pr.8 (Deceleration time) set time to accelerate the frequency to the value set by Pr.20 (Acceleration/deceleration reference frequency), the maximum frequency I need is just 20 Hz.
Can I set Pr.20 to 20 Hz?
Can I set Pr.20 to 20 Hz?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
Yes, you can set Pr.20 to 20 Hz.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700