FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Parameter
FAQ
Parameter
Is there any parameter that can be used to change the time before an overload trip (electronic thermal O/L relay error) occurs?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
No parameter can be used to directly set this time.
Changing Pr.9 (Electronic thermal O/L relay) changes the time.
Changing Pr.9 (Electronic thermal O/L relay) changes the time.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700