FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > CC-Link
FAQ
CC-Link
How can I read inverter faults from the programmable controller in CC-Link operation?
- Category :
Answer
Create a ladder program to read inverter faults on the programmable controller.
Set the instruction code (H74-H77) and turn ON the instruction code execution request RYF.
Identify the fault record from the read code.
Set the instruction code (H74-H77) and turn ON the instruction code execution request RYF.
Identify the fault record from the read code.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700