FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-Configurator
FAQ
FR-Configurator
Can I use the FR Configurator FR-SW3-SETUP-WJ to operate the inverter?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
The FR Configurator FR-SW3-SETUP-WJ can only allow for test operation.
Since this is a tool to support the system launch and maintenance, it is not designed for actual operation.
Since this is a tool to support the system launch and maintenance, it is not designed for actual operation.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700