Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21919
  • Release Date : 2018/08/22 16:30
  • Print

FR-PU04

I want to use the FR-PU04 used with the 500 series with the 700 series.
Can I set parameters that were not used with the 500 series by the FR-PU04?
Category : 

Answer

While the FR-PU04 does not display parameter names, it displays parameter numbers and you can set them.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries