FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > 12-bit digital input
FAQ
12-bit digital input
Is the setting range 0 to 400 Hz for each of BCD code and binary code inputs?
I am considering to digitally change the rotations per minute by connecting the motor with a programmable controller. Can I change it without stopping the motor?
I am considering to digitally change the rotations per minute by connecting the motor with a programmable controller. Can I change it without stopping the motor?
- Category :
Answer
You can set both the BCD code and binary code inputs within the range from 0 to 400 Hz.
You can set the bias and gain in 0.01 Hz units.
For BCD input, when the bias is 0 Hz and gain is 120 Hz, the resolution of the input command value is 120 Hz/999 = 0.12 Hz.
By setting Pr.305 = 0, the inverter constantly accepts setting frequency data input from the digital signal input terminal.
You can set the bias and gain in 0.01 Hz units.
For BCD input, when the bias is 0 Hz and gain is 120 Hz, the resolution of the input command value is 120 Hz/999 = 0.12 Hz.
By setting Pr.305 = 0, the inverter constantly accepts setting frequency data input from the digital signal input terminal.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Plug-in option
- Series
- FR-A500