Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21003
  • Release Date : 2018/08/22 16:25
  • Print

FR-A8AZ

Is the motor thermistor function of the A8AZ available for the SF-VR?
Category : 

Answer

Not available. When using the motor thermistor function, use the dedicated motor V5RU with a thermistor.
Product Name
Inverter, magnet motor drive
Product Category
Plug-in option
Series
Option
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?