Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21959
  • Release Date : 2018/08/22 16:30
  • Print

Concurrent monitoring of running frequency, output voltage, and output current

I want to output signals of the running frequency, output voltage, and output current from the inverter to an external monitoring device simultaneously. How can I do this?
Can I use the plug-in option FR-A5AY to implement this monitoring?
The externally output signals are 4 to 20 mA, 0 to 5 (10) V.
Category : 

Answer

Add an analog output by the FR-A5AY.
Monitor the three output; output AM (0 to 5 (10) V) and optional 4 to 20 mA, and 0 to 5 (10) V.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-F500, FR-A500
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?