FAQ
FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > Extension of cable of the Display Unit (Model: EMU4-D65).
FAQ
Extension of cable of the Display Unit (Model: EMU4-D65).
Is it possible to extend a cable for connecting Energy Measuring Unit (Model: EMU4-**)and Display Unit (Model: EMU4-D65) for the Energy Measuring Unit?
Answer
It is possible to extend using an extension cable (Model: EMU2-CB-T1M, EMU2-CB-T5M, EMU2-CB-T10M).
Secure the total length of the extension cable is less than 10 meters.
Secure the total length of the extension cable is less than 10 meters.
- Product Name
- Energy Measuring Units
- Series
- EcoMonitor Plus
May I have your opinion?
Related FAQ
- As to connecting an Extension Unit for an Insulation Monitor Model (Model: EMU4-LG1-MB).
- Method for measuring a circuit over 600A (EcoMonitorPlus/Light).
- Method for creating a daily/monthly report using logging data (Model: EMU4-LM).
- As to settings for EcoMonitorPlus (Model: EMU4-BM1-MB, EMU4-HM1-MB, EMU4-LG1-MB, EMU4-A2, EMU4-VA2, EMU4-AX4, EMU4-PX4).
- As to the current sensor usable for the EcoMonitorPlus (Model: EMU4-BM1-MB, EMU4-HM1-MB, EMU4-A2, EMU4-VA2).