FAQ
FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > MEASURE LED not blink (EcoMonitorPlus).
FAQ
MEASURE LED not blink (EcoMonitorPlus).
What cause assumed for no blink of MEASURE LED?
Answer
MEASURE LED lights while measuring electric power over 0.4% of the total load power. Check below points:
1. Is voltage wiring connected?
2. Are the transfix direction of current sensor, connection of k, l terminals reversed?
1. Is voltage wiring connected?
2. Are the transfix direction of current sensor, connection of k, l terminals reversed?
- Product Name
- Energy Measuring Units
- Series
- EcoMonitor Plus
May I have your opinion?
Related FAQ
- As to changing location of the decimal point and units of the measured value.
- As to compensation for power failure of Logging Unit for the Energy Measuring Unit.
- As to batch storing of data file (EcoWebServerIII).
- As to the current sensor usable for the EcoMonitorPlus (Model: EMU4-BM1-MB, EMU4-HM1-MB, EMU4-A2, EMU4-VA2).
- As to logging period of the internal memory of the main unit.