Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22178
  • Release Date : 2018/08/27 16:41
  • Update : 2020/04/10 16:56
  • Print

Difference between measurement value of active power and calculated power value obtained from current, voltage and power factor (ME96SS series).

The displayed active power is different from the active power that is calculated by multiplying the displayed current, voltage, and power factor. (The power value is small.)
Category : 

Answer

When the AC waveform distorted due to harmonics, the value changes.
(For AC without harmonics, the calculated value will match with the displayed value.)
At the time of checking harmonics, please set “on” for the harmonics display on the “Set-up menu 3”.
Product Name
Electronic Multi-Measuring Instrument
Series
ME96SS series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?