Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22181
  • Release Date : 2018/08/27 16:41
  • Update : 2020/04/10 17:05
  • Print

Setting for communication (ME96SS series).

What items should be set for communication?
Category : 

Answer

1) For the main body of ME96: Please set the following values on the “Set-up menu 2”.

In case of MODBUS RTU
 
Set-up menu No.
Setting items
Factory default settings
SSHB
SSRB
SSEB
(A)
2.2.
Address
1
(B)
 
2.2.1.
Baud rate
19.2 kbps
(C)
 
2.2.2.
Parity
EVEn
(D)
 
2.2.3.
Stop bit
1
It is necessary that the settings of (B) to (D) mentioned above correspond to the settings of the upper system.
Please set the values so that there is no overlap of the address in the same system.

In case of MODBUS TCP
 
Set-up menu No.
Setting items
Factory default settings
SSHB
SSRB
SSEB
(A)
2.4.
IP address
192.168.3.10
-
(B)
Sub-net mask
255.255.255.0
-
(C)
Use/non-use of a default gateway
oFF (Non-use)
-
(D)
Default gateway
127.0.0.1
-
After changing the set values, please perform the communication reset (Set-up menu: 2.4).

In case of CC-Link
 
Set-up menu No.
Setting items
Factory default settings
SSHB
SSRB
SSEB
(A)
2.3.
Station No.
1
-
(B)
 
2.3.1.
Communication speed
156 kbps
-
(C)
 
2.3.2.
Communication version
1.10
-
After changing the set values, please perform the communication reset (Set-up menu: 2.3.3).
It is necessary that the settings of (B) and (C) mentioned above correspond with the settings of the upper system.

In detail, please refer to the section 3 of the User’s Manual.
 
Product Name
Electronic Multi-Measuring Instrument
Series
ME96SS series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?