FAQ
FAQAbout Products
- FAQ > Low-voltage Power Distribution Products > Power Management Meters > Electrical Indicators > Active energy (lower digit indication) display upon communication test of MODBUS RTU/TCP communication (ME96SS series).
FAQ
Active energy (lower digit indication) display upon communication test of MODBUS RTU/TCP communication (ME96SS series).
When the active energy setting is set to 12-digit display on the communication test mode, how is the displayed value?
Answer
Regardless of setting, the value of the default digit length is replied.
When the register address “1304” for 6-digit display is set, the value varies with the full load.
As for the register address with a fixed unit, the value is displayed with 9-digit.
Register address for 9-digit display: “1309”, “1408” and “1426”
Register address for 9-digit display: “1309”, “1408” and “1426”
In detail, please refer to this category No.5.
- Product Name
- Electronic Multi-Measuring Instrument
- Series
- ME96SS series
May I have your opinion?
Related FAQ
- Replied value on the communication operation test of test mode (ME96SS series).
- Connectable number of MODBUS RTU (ME96SS series).
- Concurrent-use of MODBUS RTU and CC-Link.
- Register address for active energy monitors in the MODBUS RTU communication (ME96SS series).
- The operating/storage temperature and humidity