FAQ


FAQAbout Products
- FAQ > Robots > Industrial/Collaborative Robots-MELFA > Vertical type robot > The hand does not move properly (Electric operated hand).
FAQ
The hand does not move properly (Electric operated hand).
The hand does not move properly
The hand operation screen is not displayed on the TB.
(Electric operated hand)
The hand operation screen is not displayed on the TB.
(Electric operated hand)
Answer
Cause:
- Wire breakage on the hand signal line.
- The electronic hand controller(manufactured by TAIYO Ltd.) has failed.
- Faulty connection in the cables that run between devices.
- The software version on the TB and robot controller is not compatible with the electric operated hand.
- The user is trying to use the electric operated hand on a model that is not compatible with the electric operated hand.
Measures:
- Check the connections.
- Check the condition of the hand input/output signal.
- Check the mating condition of the cables that run between devices.
- Check whether the software version is compatible or not.
- Check the model compatibility.
- Product Name
- Industrial Robots MELFA
- Series
- FR Series
F Series