FAQ


FAQAbout Products

- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > Screen burn-in of the rugged model
FAQ
Screen burn-in of the rugged model
When the rugged model is used, can screen burn-in occur if the same screen continues to be displayed?
Answer
If the same screen continues to be displayed on the rugged model, a screen burn-in may occur.
Use the screen saver function to prevent a screen burn-in.
Use the screen saver function to prevent a screen burn-in.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Rugged model
- Series
- GOT2000 Series