FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > Vertical installation of the rugged model
FAQ
Vertical installation of the rugged model
Can the rugged model be used vertically?
Answer
The rugged model can be used vertically.
An arrow instructing the vertical installation is shown on the back of the GOT. Install the GOT vertically in the direction of the arrow.
An arrow instructing the vertical installation is shown on the back of the GOT. Install the GOT vertically in the direction of the arrow.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Rugged model
- Series
- GOT2000 Series