FAQ


FAQAbout Products

- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > Effect of attaching the protective cover for oil to the rugged model
FAQ
Effect of attaching the protective cover for oil to the rugged model
What is the effect of attaching the protective cover for oil to the rugged model?
Answer
Attaching the protective cover for oil to the rugged model improves oil resistance.
Because oil such as cutting oil contains a small amount of additives, the oil resistance of the protective cover cannot be specified. Before using the protective cover for oil, test it in the operating environment to determine the usability.
Because oil such as cutting oil contains a small amount of additives, the oil resistance of the protective cover cannot be specified. Before using the protective cover for oil, test it in the operating environment to determine the usability.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Rugged model, option (protective cover for oil)
- Series
- GOT2000 Series