FAQ


FAQAbout Products

- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > Controllers connectable to the rugged model
FAQ
Controllers connectable to the rugged model
What controllers are connectable to the rugged model?
Answer
The controllers connectable to the rugged model are the same as those of the GT25 wide model.
For the details, refer to the following.
GT Designer3 (GOT2000) Screen Design Manual (SH-081220ENG-W)
"12.2.1 List of [Type] and controllers"
For the details, refer to the following.
GT Designer3 (GOT2000) Screen Design Manual (SH-081220ENG-W)
"12.2.1 List of [Type] and controllers"
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Rugged model, peripheral
- Series
- GOT2000 Series