Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23707
  • Release Date : 2018/09/19 17:16
  • Print

The viewpoint of the instantaneous factor operating characteristics graph

What does 100% on the horizontal axis of the instantaneous factor operating characteristics graph mean?
Category : 

Answer

It means multiples of the settling value. For example, when an instantaneous factor operation settling value of a relay is 30 A, 100% is read as 30 A.
Product Name
Protection Relay
Series
MELPRO-A Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?