Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23709
  • Release Date : 2018/09/19 17:16
  • Print

The application of the overcurrent relay

Is that operable if one unit is connected to R-phase and another unit is connected to T-phase?
Category : 

Answer

It is possible. Connect R-phase to the terminal for R-phase of the relay, and T-phase to the terminal for T-phase of the relay. And the direction of a current from the CT must be aligned for R-phase and T-phase respectively.
Product Name
Protection Relay
Series
MELPRO-A Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?