FAQ


FAQAbout Products
- FAQ > Industrial Computer > Industrial Computer MELIPC > MI5122-VW > Regarding failure of automatic restart when Windows of MI5122-VW is frozen
FAQ
Regarding failure of automatic restart when Windows of MI5122-VW is frozen
MI5122-VW's Windows was frozen but Windows did not restart automatically. What could be the cause?
- Category :
Answer
Windows automatic restart function runs when Windows stops due to the blue screen of Windows.
Even if Windows is frozen on the display, the Windows system may continue to operate.
In that case, Windows automatic restart Function does not run.
Even if Windows is frozen on the display, the Windows system may continue to operate.
In that case, Windows automatic restart Function does not run.
- Product Name
- MELIPC
- Series
- MI5000