FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the FX5UC CPU module/Intelligent Function module Power Cable
FAQ
Regarding the FX5UC CPU module/Intelligent Function module Power Cable
What is the cable type name of the power cable (Red, black and green) used for the FX5UC CPU module or Intelligent Function module?
- Category :
-
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > CPU Module
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Network/Communication
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Motion/Positioning
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Analog
Answer
The model name of the power cable is FX2NC-100MPCB. It is included with the FX5UC CPU module and intelligent function modules that require power from the power connector.
- Product Name
- FX5UC,FX5-CCLIEF,FX5-CCL-MS,FX5-CCLGN-MS,FX5-40/80SSC-S,FX5-40/80SSC-G,FX5-20PG-P/D,FX5-8AD,FX5-4LC
- Product Category
- CPU Module,Analog,Motion/Positioning,Network/Communication
- Series
- MELSEC iQ-F Series