Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22285
  • Release Date : 2018/08/30 13:55
  • Print

Regarding the type of battery which can be used with the CPU module.

What is the model name of the battery that can be used with the CPU module?
Category : 

Answer

FX3U-32BL can be used.                                                                                          
The battery is not included with the CPU module during factory shipment.
The battery can be used to increase the capacity of the latch device/label, as well as to maintain the clock data during power interruption.
Product Name
FX5U, FX5UC
Product Category
CPU Module, Options
Series
MELSEC iQ-F Series

May I have your opinion?

Inquiries