FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the function of a special relay.
FAQ
Regarding the function of a special relay.
Which relay is the "Always ON" relay?
Answer
SM400 and SM8000.
※FX compatible area(SM8000~, SD8000~) is available for the special relay and special device.
※FX compatible area(SM8000~, SD8000~) is available for the special relay and special device.
- Product Name
- FX5U,FX5UC,FX5UJ,FX5S
- Product Category
- CPU Module
- Series
- MELSEC iQ-F Series