Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22288
  • Release Date : 2018/08/30 13:55
  • Print

Regarding the function of a special relay.

Answer

SM400 and SM8000.
※FX compatible area(SM8000~, SD8000~) is available for the special relay and special device.
Product Name
FX5U, FX5UC
Product Category
CPU Module
Series
MELSEC iQ-F Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?