FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > CPU Module > Regarding a mismatch found in the monitoring function of GX Works3
FAQ
Regarding a mismatch found in the monitoring function of GX Works3
A mismatch was found between the actual operation of the PLC and the monitor status of GX Works3.
Is there a solution to fix the mismatch?
Is there a solution to fix the mismatch?
Answer
Perform "Rebuild All" and initialize the memory before writing to the PLC.
"Rebuild All" converts the entire project and "Convert" only coverts the modified part of the program.
For further details please refer to GX Works3 Operating Manual.
"Rebuild All" converts the entire project and "Convert" only coverts the modified part of the program.
For further details please refer to GX Works3 Operating Manual.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Engineering Software
- Series
- MELSEC iQ-F Series