FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > CPU Module > Regarding the maximum number of controllable axes of the bulit-in positioning function
FAQ
Regarding the maximum number of controllable axes of the bulit-in positioning function
What is the maximum number of the axes that can be controlled with the built-in positioning function of FX5 CPU module?
Answer
Up to 4 axes can be controlled. Please use a transistor output type CPU module.
(By adding a high speed pulse input/output module,
maximum 12 axes (CPU built-in 4 axes+expansion 2 axes×4 modules) can be configured.
(By adding a high speed pulse input/output module,
maximum 12 axes (CPU built-in 4 axes+expansion 2 axes×4 modules) can be configured.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Motion/Positioning
- Series
- MELSEC iQ-F Series