Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22302
  • Release Date : 2018/08/30 13:55
  • Print

Regarding MODBUS/TCP communication of the built-in Ethernet function

Answer

1.Master station can communicate with the slave stations using the predefined protocol support function.
2. Slave station communication with the master station is supported with CPU firmware Ver.1.060 or above and GX Works3 Ver. 1.040S or above.
Also, it is possible to use the master or slave at the same time with a single FX5U CPU module.
Product Name
FX5U, FX5UC
Product Category
CPU Module, Network/Communication
Series
MELSEC iQ-F Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?