- No : 22302
- Release Date : 2018/08/30 13:55
-
Print
Regarding MODBUS/TCP communication of the built-in Ethernet function
Does built-in Ethernet port support MODBUS/TCP communication function?
- Category :
-
Answer
1.Master station can communicate with the slave stations using the predefined protocol support function.
2. Slave station communication with the master station is supported with CPU firmware Ver.1.060 or above and GX Works3 Ver. 1.040S or above.
Also, it is possible to use the master or slave at the same time with a single FX5U CPU module.
- Product Name
- FX5U, FX5UC
- Product Category
- CPU Module, Network/Communication
- Series
- MELSEC iQ-F Series