FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > High-Speed Counter > Regarding changing the current value of the high-speed counter.
FAQ
Regarding changing the current value of the high-speed counter.
How can the current value of the high speed counter with high-speed I/O function be changed?
Answer
To rewrite the current value, arbitrary values can be written using the DHCMOV instruction.
(Example) Set the current value of the high-speed counter ch1 to 0.[DHCMOV K0 SD4500 K0]
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, High-Speed Counter
- Series
- MELSEC iQ-F Series
May I have your opinion?
Related FAQ
- Regarding the maximum number of channels of high-speed counters
- Regarding the number of available channels of the built-in high speeed counters.
- Regarding model name of CC-Link cables
- Regarding the settings of built-in analog function of FX5U CPU module
- Regarding selection of FX3 intelligent function modules on the module configuration diagram of GX Works3