FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > CPU Module > Regarding I/O assignment on the module configuration diagram of GX Works3
FAQ
Regarding I/O assignment on the module configuration diagram of GX Works3
Is it possible to check the I/O assignment of CPU or I/O extension modules on module configuration diagram of GX Works3?
Answer
While the module configuration window is being displayed,
the I/O assignment can be checked by selecting the following options from the menu bar:
[Edit]→[XY Assignment Display]
the I/O assignment can be checked by selecting the following options from the menu bar:
[Edit]→[XY Assignment Display]
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, I/O Module, Engineering Software
- Series
- MELSEC iQ-F Series