Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22308
  • Release Date : 2018/08/30 13:55
  • Update : 2022/12/22 10:13
  • Print

Regarding the link refresh settings of FX5-CCL-MS

When setting the link refresh settings from GX Works3 by configuring the FX5-CCL-MS (CC-Link system master/intelligent device) as a master station, is it possible to use latch devices or I/O devices (X/Y) for link refresh devices?
Category : 

Answer

It is possible to use latch devices or I/O devices (X/Y) for link refresh devices.
However, when using I/O devices (X/Y), use  I/O numbers (such as X1000 ~/Y1000~) that are not assigned to actual control.
Also, you can check the device allocation settings for refresh devices in GX Works3 by following the steps below.
 View > Docking Window > Device Assignment Confirmation of GX Works3 menu and specify the appropriate module number in [Mounting Position No.].
However, make the network configuration settings and link refresh settings in the CC-Link parameters beforehand.
Product Name
FX5-CCL-MS
Product Category
CPU Module, Network/Communication, Engineering Software, GX Works3
Series
FX5U,FX5UC,FX5UJ
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?