FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > High-Speed Counter > Regarding the frequency of high-speed counters
FAQ
Regarding the frequency of high-speed counters
Which frequencies can be used for the FX5 CPU high-speed counters?
Answer
The maximum frequency of the FX5U/FX5UC CPU module is 200kHz and the maximum frequency of the FX5S/FX5UJ CPU module is 100 kHz.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, High-Speed Counter
- Series
- MELSEC iQ-F Series
May I have your opinion?
Related FAQ
- Regarding changing the current value of the high-speed counter.
- Regarding the number of available channels of the built-in high speeed counters.
- Regarding the maximum number of channels of high-speed counters
- Regarding the settings of built-in analog function of FX5U CPU module
- Regarding 2-axis synchronous control