FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the built-in analog input/output function
FAQ
Regarding the built-in analog input/output function
Is it possible to perform analog input/output operations with the FX5U/FX5UC CPU module alone?
Answer
FX5U CPU module has 2 built-in voltage input channels (DC0~10V) and 1 built-in voltage output channel (DC0~10V).
If an external resister is connected, the module can also support current input (DC4~20mA).
For further details, please refer to MELSEC iQ-F FX5 User's Manual (Analog Control - CPU module built-in, Expansion adapter).
Because the FX5UC CPU modules do not have a built-in analog function, please use an analog adapter or intelligent function module.
If an external resister is connected, the module can also support current input (DC4~20mA).
For further details, please refer to MELSEC iQ-F FX5 User's Manual (Analog Control - CPU module built-in, Expansion adapter).
Because the FX5UC CPU modules do not have a built-in analog function, please use an analog adapter or intelligent function module.
- Product Name
- FX5U, FX5UC
- Product Category
- CPU Module, Analog
- Series
- MELSEC iQ-F Series